Technical FAQs

Ask a Question

Is it possible to do Ethernet I/O scanning with the Advantys OTB1E0DM9LP Ethernet module?

Release Notice

Dick, can you republish the following FAQ's that were archived and set the date out for more than a year.

Goals and Symptoms

Yes, you will need to set up the Ethernet I/O scanner in the following way. For this example we are using a Momentum Ethernet processor and Concept.
NOTE: You will want to make sure that the executive in the PLC is up to the latest revision, if not you will not be able to I/O scan.

Causes and Fixes

As noted below the Read Ref Slave address must be 400001 and the Write Ref Slave must be 400101.


Legacy KB System (APS) Data: RESL174918 V4.0, Originally authored by DiSa on 04/10/2007, Last Edited by BrWa on 06/13/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?