Technical FAQs

Ask a Question

How do you write to the TWDXCPMFK32 Twido 32k backup cartridge?

Goals and Symptoms

To give a steps for backing up your program into the backup cartridge.

Causes and Fixes

Here is the step by step procedure for performing the backup .
Note: Step 4 where it says "Controller" it may say "PLC"

Legacy KB System (APS) Data: RESL174802 V2.0, Originally authored by DiSa on 06/08/2012, Last Edited by BrWa on 06/08/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?