Technical FAQs

Ask a Question

What are the dimensions for the 19 inch B800 series to Quantum Swing Arm assembly?

The dimensional drawing for the 19" B800 Quantum Swing Arm is attached below. The Swing Arm is available in both aluminum and painted steel.
19" Swing Arm part#'s:

990QFCSWM19A (aluminum)
990QFCSWM19S (steel)

19InchAcad2000 .pdf19Inch prototype acad2000 12Nov04.zip


Legacy KB System (APS) Data: RESL174744 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?