Technical FAQs

Ask a Question

What are the dimensions for the 27 inch B800 series to Quantum Swing Arm assembly?

The dimensional drawing for the 27" B800 series to Quantum Swing Arm assembly is attached below. The Swing Arm is available in both aluminum and painted steel.
27" Swing Arm part #'s:

990QFCSWM27A (aluminum)
990QFCSWM27S (steel)



27Inch Acad2000 Model (1).pdf 27Inch Acad2000.zip

Was this helpful?
What can we do to improve the information ?