Technical FAQs

Ask a Question

Is there an Advantys STB Modbus NIM available ?

No, there is no Modbus NIM available for Advantys. However, a new feature was introduced in Advantys configuration software version 2.0 where you can set the NIM in permanent test mode. Select the option for persistent test mode under the menu Island > Test Mode Settings. Now the island I/O can be controlled by a HMI or any Modbus master connected through the configuration port.


Legacy KB System (APS) Data: RESL174738 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?