Technical FAQs

Ask a Question

Is it possible to use data types known in Unity Pro?

In UAG a file is available which contains the Unity Pro DDTs: <UAG Install Dir>\DB\UnityProLibset.dty.
This file can be imported in the SCoD Editor with File / Import Data Types. In the dialog the necessary data types have to be selected.
Examples of data types: BoolArr32, INTARR8, WordArr5.


Legacy KB System (APS) Data: RESL174273 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?