Technical FAQs

Ask a Question

How many ASi master modules can I configure in a Twido application?

On the Twido controllers that support expansion bus, a maximum of two ASi master modules are supported.


Legacy KB System (APS) Data: RESL174109 V1.0, Originally authored by on , Last Edited by on
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?