Technical FAQs

Ask a Question

Why can't I copy 984LL networks from one Concept project to another Concept project?

There is a line that can be added to the Debug section of the concept.ini file to allow this. The concept.ini file resides in the \windows or \winnt folder.

[Debug]

; allows for copy/pasting 984LL Nets
RemoveLL984NetworksFromClipboard=0


Legacy KB System (APS) Data: RESL174068 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?