Technical FAQs

Ask a Question

How is the system timer defined in Unity Pro?

Unity provides an incremental timer with 100 msec update in system word %SD18.
This differs from Concept which located the system timer on a user defined register word (16Bit) which was incremented every 10msec.

 


Legacy KB System (APS) Data: RESL174021 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?