Technical FAQs

Ask a Question

When I tried to create a Project Archive in Unity v2.0, the Archive option on the File menu grayed out? Why?

If you imported the project in XEF format, or opened an STU file, you must first perform a Build -> 'Rebuild All Project', before the File -> 'Archive' selection becomes available. A Unity archive file is approximately 50 times more compressed the native STU file format.,


Legacy KB System (APS) Data: RESL173938 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?