Technical FAQs

Ask a Question

PL7PRO V4.5 SP2 _ Installation and software license retrieval

Release Notice

PL7V4.5 Service Pack 2 (SP2) can only be installed on a workstation with version V4.5 of PL7 Pro, Junior, or Micro.

Goals and Symptoms

Depending from the previous PL7 installed versions and PC configuration , you may have lost the software license when installing PL7V4.5 product . The symptoms are an error message " transferred rights " or " you have to registrate your version until 21 days " when launching PL7 after installation . This resolution explain the installation of Service Pack2 depending of your already PL7 installed PRODUCTS .

Causes and Fixes


Case 1: If you get a PL7 V4.5 product including Service Pack 1:
1 - Don't install the Service Pack 1
2 - Download the Service Pack 2 from WWW. TELEMECANIQUE.COM web site under PRODUCTS / PRODUCTS index / Sotware Tools
/ PL7 => Soft./Firmw. item
3 - Unzip the PL745SP2.ZIP file in a temporary folder
4 - Refer to the installation procedures:
- Chapter 1: Installation of a new product PL7 V4.5 SP2
- Chapter 2: Installation of PL7 V4.5 SP2 update PRODUCTS, expired subscription or upgrade

Case 2: If you get a PL7 V4.5 product including Service Pack 2:
- Refer to the installation procedures:
- Chapter 1: Installation of a new product PL7 V4.5 SP2
- Chapter 2: Installation of PL7 V4.5 SP2 update PRODUCTS, expired subscription or upgrade

CHAPTER1 - Installation of a new product PL7 V4.5 SP2
1 - Install the programming software PL7 V4.5
- Run F:\PL7V45\setup.exe to install the application, F being the CD-ROM drive.
2 - Install the SP2 software
- Run ...\PL7V45SP2\setup.exe to start the installation whether from the CD-ROM drive or from the temporary folder
- Once the software is installed, the PL7 application is identified as PL7 V4.5/SP2, as displayed in the "About..." box
in the main menu. ".
3. You have 21 days to register through the registration tool PL7 V4.5


CHAPTER2 - Installation of PL7 V4.5 SP2 update PRODUCTS, expired subscription or upgrade

2.1 on a PL7 version V4.4




1. Check that the PL7 version to V4.4 has been authorized on the PC.
- If not, authorize it before continuing.
2. Install the PL7 V4.5 software application by following the installation instructions.
- Run F:\PL7V45\setup.exe to install the application, F being the CD-ROM drive.
3. Install the SP2 software
- Run ...\PL7V45SP2\setup.exe to start the installation whether from the CD-ROM drive or from the temporary folder
- Once the software is installed, the PL7 application is identified as PL7 V4.5/SP2, as displayed in the "About..." box
in the main menu. ".
4. You obtain permanent user rights for the PL7 V4.5 and SP2 software application.

2.2 _On a PL7 version prior to V4.4

1. Check that the PL7 version prior to V4.4 has been installed on the PC.
- If not, install it before continuing
2. Install the PL7 V4.5 software application by following the installation instructions.
- Run F:\PL7V45\setup.exe to install the application, F being the CD-ROM drive.
3. Install the SP2 software
- Run ...\PL7V45SP2\setup.exe to start the installation whether from the CD-ROM drive or from the temporary folder
- Once the software is installed, the PL7 application is identified as PL7 V4.5/SP2, as displayed in the "About..." box
in the main menu. ".
4. You have 21 days to register through the registration tool PL7 V4.5


Legacy KB System (APS) Data: RESL173913 V1.0, Originally authored by on , Last Edited by on
Related ranges: PL7
Was this helpful?
What can we do to improve the information ?