Technical FAQs

Ask a Question

Which Transparent Ready product and service should I use if I have a device that only supports 1 TCP socket and I have to make multiple read requests?

Consider the Quantum Ethernet IO Scanner using the 140NOE771x1. Other devices open a TCP Socket for each message transaction The Quantum NOE using IO Scanner will keep the TCP Socket open and make repeated requests on that same TCP Socket.

Was this helpful?
What can we do to improve the information ?