Technical FAQs

Ask a Question

I have Altivar 38 and 58 Drives with an embedded VW3A58310 cards. What ModbusTCP services does this support?

The Altivar 38 and 58 Drives with the embedded VW3A58310 cards support being a Modbus Server, FDR client, BootP client and embedded web diagnostics.


Legacy KB System (APS) Data: RESL173858 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?