Technical FAQs

Ask a Question

What is the maximum message size that OFS can accomodate on TCP/IP?

OFS supports 1,022 byte Read messages and 1,008 Write messages, maximum, using the UNITE protocol.


Legacy KB System (APS) Data: RESL173821 V1.0, Originally authored by on , Last Edited by on
Related ranges: OFS
Was this helpful?
What can we do to improve the information ?