Technical FAQs

Ask a Question

Can I configure a Unity Premium PLC with an initial configuration using USB instead of Unitelway?

Yes. You can write an initial configuration on a Unity Premium PLC with the USB interface for those supported controllers with a USB interface like the TSXP575634.


Legacy KB System (APS) Data: RESL173818 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?