Technical FAQs

Ask a Question

I have had communication problems after downloading my XBTL-1000 application to my Magelis and my communications are correctly configured. What can I do?

Try saving your XBTL-1000 application under a different filename to re-establish the database. Then download the application to the Magelis.


Legacy KB System (APS) Data: RESL173815 V1.0, Originally authored by on , Last Edited by on
Related ranges: XBT K, XBT B, XBT A, XBT V...
Was this helpful?
What can we do to improve the information ?