Technical FAQs

Ask a Question

Can I log trend data from my FactoryCast module to a database, or retrieve it as a file?

Typically no, you cannot log FactoryCast module trend data to a file. The data is presented to the interface via volatile memory and is only captured on screen. Should you need to capture trend data to a file, use the FactoryCast HMI module (Quantum 140NWM10000 or Premium TSXWMY100), to push data to a supported SQL database.


Legacy KB System (APS) Data: RESL173804 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?