Technical FAQs

Ask a Question

Devices on my LAN use both Ethernet II and IEEE 802.3 frame formats. How do I configure this?

No reconfiguration is necessary as long as those devices communicating in each of the frame formats matches the frame format of the listener. Both frame formats can coexist on the same network. Devices should communicate with in-kind frame formats.


Legacy KB System (APS) Data: RESL173803 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?