Technical FAQs

Ask a Question

If I connect my 10BaseT, half duplex Ethernet device such as a Momentum CPU to an Ethernet switch, do I eliminate collisions?

No, You do not eliminate collisions. As the M1 being half duplex, and the Ethernet switch negotiating a matched 10 Mbs half duplex connection, this remains a collision diameter network of 2 devices. Either the half duplex device can transmit, or the switch can transmit, but not both simultaneously. Only full duplex devices can communicate simultaneously with Ethernet full duplex capable switches.


Legacy KB System (APS) Data: RESL173802 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?