Technical FAQs

Ask a Question

Can I configure my PC or Server to a Multicast address range to participate as a Global Data subscriber (Real Time Publish Subscribe)?

No. Multicast addressing is not permitted on PC's. Only devices configured to listen on the published Multicast IP can participate. Microsoft Windows does not permit assigning a Multicast IP address (224.0.0.0 - 239.255.255.255) to a PC.


Legacy KB System (APS) Data: RESL173800 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?