Technical FAQs

Ask a Question

What is the most secure method of Remote Access to my PLC?

The most secure method is to dial into a Remote Access Server (RAS), that requires authentication with Dial-Back access. This assures the once authentication has been validated, that a predefined telephone number will be dialed back for a connection.


Legacy KB System (APS) Data: RESL173799 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?