Technical FAQs

Ask a Question

I have to run power cabling in the same enclosure with Ethernet LOW_VOLTAGE data cabling. What practices should I follow?

If your installation permits it, consider running data cabling in conduit to serve as an electrostatic shield. Should that not be an available option, run LOW_VOLTAGE data cable in right angle raceways to power cable to minimize high frequency RF interference from power cable to data cable.


Legacy KB System (APS) Data: RESL173798 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?