Technical FAQs

Ask a Question

What are the pinouts for the M12 connector on my ConneXium IP67 Ethernet switch?

The connectors shown below are used in the IP67 ConneXium TCS ESU 051 F0 switch.


Note that if the other end is RJ45, the pinouts on the RJ45 end are 1 (TD+), 2 (TD-), 3 (RD+) and 6 (RD-).


Legacy KB System (APS) Data: RESL173796 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?