Technical FAQs

Ask a Question

Which Transparent Ready services do the Altivar 38 and Altivar 58 support?

The Altivar 48 and 58 support:
- Modbus server on TCP 502
- FDR client with DHCP option 61 (client unique identifier), role name
- BootP client
- Embedded Diagnostics


Legacy KB System (APS) Data: RESL173793 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?