Technical FAQs

Ask a Question

Which Transparent Ready ConneXium Gateways support embedded Web diagnostics?

Embedded Web Diagnostics are supported only in the current product Modbus Plus/Ethernet 174CEV20040 gateway.


Legacy KB System (APS) Data: RESL173784 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?