Technical FAQs

Ask a Question

What is the minimum version of Concept needed to support the Quantum 140NWM100-00 FactoryCast HMI module?

Concept version 2.6 SR2 added support for the 140NWM100-00 module.
However, the 140NWM100-00 module can be added to Concept 2.6 SR1's pick list. This is done by installing an .MDC file through Concept's ModConnect Tool. The .MDC file is attached below.

NWM100_mdc.zip


Legacy KB System (APS) Data: RESL173764 V3.0, Originally authored by MiRo on 04/14/2010, Last Edited by DaSo on 02/28/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?