Technical FAQs

Ask a Question

Why won't XMIT communicate through the Quantum NOM21x Modbus port?

XMIT will only work with Modbus port one on the Quantum CPU.
The only CPUs that support XMIT communications on Modbus Port 2 are the Momentums.


Legacy KB System (APS) Data: RESL173600 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?