Technical FAQs

Ask a Question

What is the difference between the AS-B846-001 and the AS-B846-002?

The B846-001 is a voltage module.
The B846-002 is a current module..

No, they are not interchangeable.


Legacy KB System (APS) Data: RESL173598 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?