Technical FAQs

Ask a Question

What impact does rearranging the order of the IEC sections listed in the Concept Project Browser have on the program?

Rearranging the IEC sections online through the Project Browser changes the execution order. The project and PLC status will be changed to MODIFIED and a 'download changes' will be required to restore EQUAL status.


Legacy KB System (APS) Data: RESL173263 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?