Technical FAQs

Ask a Question

Is it possible to write a command line to export a Concept project directly ?

Yes, to export a Concept project go to <Start><run> and type:

c:\concept\dbconv.exe /Y c:\concept\testprj\testprj.prj

This automatically exports the testprj project that resides in c:\concept\testprj to an .ASC file. The /Y switch skips any warnings.
NOTE: DFBs can also be exported by specifying the .dfb extension and can also be imported.

Yes, to import a Concept project go to <Start><run> and type:

c:\concept\dbconv.exe /Y c:\concept\testprj\testprj.ASC

This automatically imports the testprj project that resides in c:\concept\testprj.

Was this helpful?
What can we do to improve the information ?