Technical FAQs

Ask a Question

Can the Magelis system pages be modified in XBTL1000?

Goals and Symptoms

Can the Magelis system pages be modified in XBTL1000?

Causes and Fixes


In general No, the system pages cannot be modified.

Below is a summary of the available System pages.




Many users wish to modify the pages by deleting particular functions they do not want to be available from that page, or to copy functionality from a System page to an Application page. An example would be to copy the Terminal Parameters button from one page to another. This type of modification is not possible.



Minor modifications however are possible but not recommended. Below is a System page that is about to have a function description text field modified.


Legacy KB System (APS) Data: RESL173033 V1.0, Originally authored by on , Last Edited by on
Related ranges: XBL
Was this helpful?
What can we do to improve the information ?