Technical FAQs

Ask a Question

Using Concept how can I tell what project resides in the PLC?

There are two ways to do this.
To view the name of the project last downloaded to the PLC, first connect to the PLC. From the Online menu select <Object information>. The name and date of the last project downloaded, as well as all Derived Function Blocks contained in the project, will be displayed.



The second way is to use the PRJ_VERS function block. This gives month, day, year, hour, minute, second and project name information.


Legacy KB System (APS) Data: RESL173029 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?