Technical FAQs

Ask a Question

How is Bandwidth Monitoring computed in the 140NOE771x1 module?

The bandwidth monitoring is based upon the percentage of maximum usage for each of the Ethernet Communication services. The maximum throughput for each service is based upon the percentage of CPU utilization with the following maximum rates:
Global Data - 800 Published Variables per second by the NOE CPU.
I/O scanner - 4200 Transactions per second by the NOE CPU.
Messaging - 410 Modbus TCP messages transacted per second by the NOE CPU.
NOE CPU - Percentage of resources idle.

The computation = ( Current Load * 100) / (Maximum Load).

Legacy KB System (APS) Data: RESL172829 V2.0, Originally authored by MiRo on 11/14/2012, Last Edited by BrWa on 11/14/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?