Technical FAQs

Ask a Question

How many operations are the Twido relay outputs rated for?

The Twido relay outputs are rated for:
- 2A/ 240 VAC or 2A/ 30 VDC (with 1800 operations/hour max) :
- electrical life : minimum 100 000 operations
- mechanical life : minimum 20 x 106 operations


Legacy KB System (APS) Data: RESL172642 V1.0, Originally authored by on , Last Edited by on
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?