Technical FAQs

Ask a Question

Is the backup battery in the TSX07 Nano field replaceable?

No. The battery in the TSX07 Nano PLCs is not field replaceable. The units have on-board EEPROM for nonvolatile program storage as well as battery backup to maintain the program in RAM for up to 30 days. In the event battery backup fails, the controller will load a saved program from EEPROM on power up.


Legacy KB System (APS) Data: RESL172528 V1.0, Originally authored by on , Last Edited by on
Related ranges: TSX07
Was this helpful?
What can we do to improve the information ?