Technical FAQs

Ask a Question

How long of an interruption in operation power can the TSX07 Nano PLCs withstand without interrupting operations?

All AC powered models of the TSX07 Nano can withstand a power interruption of less than or equal to 10 msec without interrupting operations.
All DC powered versions of the TSX07 Nano can withstand a power interruption of less than or equal to 1 msec without interrupting operations.
(reference TLXDM07DSE)


Legacy KB System (APS) Data: RESL172476 V1.0, Originally authored by on , Last Edited by on
Related ranges: TSX07
Was this helpful?
What can we do to improve the information ?