Technical FAQs

Ask a Question

Does the Global Replace feature check for duplicate coils in the ProWORX 32 programming software?

Yes. Tested using version 2.1 SP2 the Global Replace feature in ProWORX 32 does check for duplicate coils. It will replace the duplicate coil addresses, and list a notification that they are duplicate.


Legacy KB System (APS) Data: RESL172453 V2.0, Originally authored by RoAl on 02/07/2013, Last Edited by RoAl on 02/07/2013
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?