Technical FAQs

Ask a Question

What does Concept error message 'Still Processing Command - Error Id: OL9-1579' mean when trying to go on-line via Modbus Plus?

When attempting to connect via Modbus Plus, Error ID: OL9-1579 is usually caused when the "Win16 applications support" is not selected for the Virtual MBX Driver. Concept is a 16 bit Application and requires this to be selected.


Legacy KB System (APS) Data: RESL1722 V2.0, Originally authored by RiTa on 09/05/2012, Last Edited by MiOB on 09/05/2012
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?