Technical FAQs

Ask a Question

What is the baud rate of the parent/child serial I/O expansion link when using the Modicon Micro 110CPUxxxxx units?

The baud rate of the parent/child serial I/O expansion link when using the Modicon Micro 110CPUxxxxx units is 12.5k baud.


Legacy KB System (APS) Data: RESL171907 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Micro
Was this helpful?
What can we do to improve the information ?