Technical FAQs

Ask a Question

What is the maximum network length of the serial I/O expansion link supported by the 110CPUxxxxx Modicon Micro controllers?

The maximum length of the serial I/O expansion link supported by the 110CPUxxxxx Modicon Micro controllers is 1500' (or 500m).


Legacy KB System (APS) Data: RESL171905 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Micro
Was this helpful?
What can we do to improve the information ?