Technical FAQs

Ask a Question

Why isn't the .var file that is used with OFS present after importing a Concept file?

In order for the file to be created and placed in the \VAR folder on a Concept import, the flag must be set in the concept.ini file.
;ExportVariables: enable/disable variable export for OFS
ExportVariables=1

This flag must be set to 1 for the .var file to be created.


Legacy KB System (APS) Data: RESL171864 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?