Technical FAQs

Ask a Question

Is there a way to speed up the analysis on hybrid (IEC and 984LL) Concept projects when downloading or downloading changes?

IEC & 984LL hybrid projects with many variables can take a very long time to analyze due to checking for multiple coils in the IEC and 984LL sections.
After installing Patch A for Concept 2.6 SR2, there are two possibilities to speed up the analyzing in mixed projects:
- by deselecting the analyzer option Show Warnings (all analyzer warnings are eliminated).
- by setting the option SkipMultiAssignCheckIecLL984=1 in the [Debug] section of the concept.ini file.
Only the check for multiple coils in IEC/984LL sections is skipped.


Legacy KB System (APS) Data: RESL171863 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?