Technical FAQs

Ask a Question

What is the COMAND and CONTROL selections in the ETZ 410 version 1.7 used for.

Goals and Symptoms

What is the COMAND and CONTROL selections in the ETZ 410 version 1.7 used for.

Causes and Fixes

The TSX ETZ410 version 1.7 web page menu functions 'COMMAND' and 'CONTROL' are only used when the connected device has the capability to use these functions. The instructions for using these functions can be found in the assocaited user manual for the attached device (i.e., Ativar 71). These functions are not supported on Premium devices (i.e., ETY, ETZ, etc.).

Was this helpful?
What can we do to improve the information ?