Technical FAQs

Ask a Question

What does Concept's online EQUAL state mean?

The EQUAL online state in Concept means that the project files have the same version time stamps as the project in the PLC. The PLC configuration is identical between the PLC and the project.
The checksums for the 984LL and IEC code are identical.
The user defined datatypes are identical to the last time the project was opened.

NOTE: The state ram contents and discrete states are not part of the compare and are not considered in determining EQUAL status.


Legacy KB System (APS) Data: RESL171663 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?