Technical FAQs

Ask a Question

What causes an "autoexec.nt could not be used in MS-DOS and Windows applications" error message when trying to launch Concept?

One condition which can prompt this message is when the autoexec.nt is not in the windows\system32 folder but in another folder. If this is the case, simply move the autoexec.nt file to the \windows\system32 folder.


Legacy KB System (APS) Data: RESL171523 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?