Technical FAQs

Ask a Question

Direct connection of XBTG to Twido (Modbus)

Goals and Symptoms

The aim of this resolution is to give some advices for the direct connection of XBTG to Twido (Modbus)

Facts and Changes

XBTG Twido modbus RTU XBTZ968 twidosoft configuration protocol

Causes and Fixes

Please see the attached document

Attachments

(Removed File URL: 171518_8D92/direct_connection_to_twido_modbus.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/65f49ff6f75e3be1c125702900326ebf/fl_block_5/0.13E8?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL171518 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?