Technical FAQs

Ask a Question

What is the maximum length of an array or structure in Concept?

The maximum length of an array or structure used in Concept is 64Kbytes.


Legacy KB System (APS) Data: RESL171407 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?