Technical FAQs

Ask a Question

If the Ethernet connection is lost while online, when connection is re-made an error ' user already logged in' is displayed and will not allow the PC ...

Goals and Symptoms

If the Ethernet connection is lost while online, when connection is re-made an error ' user already logged in' is displayed and will not allow the PC back online

Facts and Changes

If the Ethernet connection is lost while online, when connection is re-made an error ' user already logged in' is displayed and will not allow the PC back online

Causes and Fixes

The behaviour is due to the way that the Quantum cpu communicates to to the NOE over the backplane during programming with any plc programming software package.

When the plc programming software (i,e., ProWORX,32, etc.) is connected to the plc via the NOE, the cpu opens a seperate internal programming path to connect the NOE to the cpu. The programming information is passed on to the cpu directly from the NOE independent of the physical connection.
When the connection is broken while the ProWORX is connected to the plc, the cpu does not know that the physical connection to ProWORX has been lost. Since only one programming path can be opened to the plc at any given time, any attempt to reconnect via the NOE is rejected by the cpu. However, if the NOE is lifted off of the backplane and is reseated, the cpu detects a broken connection to the NOE and resets the programming path.
This problem has been fixed in
Executive Firmware version 3.6 for the 140NOE77101
Executive Firmware version 3.5 for the 140NOE77111
Executive Firmware version 3.4 for the 140NOE77100

Note: 140NOE77110 is considered to be obsolete and has been replaced by the 140NOE77111


Legacy KB System (APS) Data: RESL171042 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?