Technical FAQs

Ask a Question

How do I activate the emulation feature in the ProWorx Plus software?

From the ProWorx Plus Network Editor, select "Alt-Q" on your keyboard. This will open the Quick Commands. Select the "Emulation" option, then "<F2> - Mode". To activate emulation select "<F2> - Running". To stop emulation select "<F3> - Stopped".


Legacy KB System (APS) Data: RESL170775 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?