Technical FAQs

Ask a Question

How do I switch between Power and State Flow in the ProWORX 32 software?

Open the Logic Editor Properties and under the Logic tab simply check off the box for State Flow. If this box is not checked off then Power Flow is activated.


Legacy KB System (APS) Data: RESL170424 V2.0, Originally authored by PeZa on 12/04/2012, Last Edited by RoAl on 12/04/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?